PCF2129 SDO and CLKOUT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF2129 SDO and CLKOUT

742件の閲覧回数
mlibhart
Contributor I

Really simple question from a hobbyist.  Is it ok to let SDO (serial data out) and the clkout float on the PCF2129 RTC if I'm not using either, or should they be tied one way or the other?  I'll be using I2C so don't need the SDO.

Thanks.

0 件の賞賛
返信
3 返答(返信)

622件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Matthew,

The SDO and CLKOUT pins of the PCF2129 device are output functions.  It is okay to leave output pins floating.

Best regards,

Tomas

0 件の賞賛
返信

622件の閲覧回数
fatihozen
Contributor IV

Hi, I have similar question, I won't use TS, SDO, INT and CLKOUT pins and ESD protection is very important on my side. What do you suggest for these pins connections ? I think it is better choice to connect them somewhere via resistors than letting float, but I need an advice here.

0 件の賞賛
返信

622件の閲覧回数
mlibhart
Contributor I

Hi Tomas,

Thanks so much for the quick reply.  Really appreciate it.

0 件の賞賛
返信