PCA9955B Short Circuit Detection Issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9955B Short Circuit Detection Issues

1,430 次查看
ricola96
Contributor I

Hello,

 

I've got a design that uses the PCA9955B and I'm having issues where there is a short circuit reported on all LEDs.

I measure the input pins of the driver and I'm reading ~3.4V but I noticed in the datasheet that if Vo >= Vth then the short circuit error happens. Vth is ~2.85V as per the datasheet.

I'm controlling my LEDs with 5V - is the intention that the LED is used to drop that 5V to something < 2.85V?

Thank you in advance.

标记 (2)
0 项奖励
回复
2 回复数

1,406 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello, could you please share your schematic?

Remember that for all unused LED outputs, the user must program their LED outputs to the ‘OFF’ state (LDRx = 00) and IREFx value to 00h, and all unused LED output pins must be pulled up to VDD with a recommended 100 k shared resistor.

Hope this helps.

0 项奖励
回复

1,396 次查看
ricola96
Contributor I

Thank you for the response, please see attached for an image of the relevant part of my schematic.

I don't have the unused outputs tied to Vdd through that resistor - but would that be causing a short error in LEDs that are there?

I can add the LED in the coming days and keep you posted as well.

0 项奖励
回复