has an LCD12864.
I can't believe there is no backlight. Have I missed something?
Hi XiangJun,
The pins in your document do not match the display ribbon or the circuit diagram on the OM13082 board.
There is no evidence of LEDA/LEDK on the OM13082 board connector. There are 20 pins on the LCD and 28 pins on the external end of the ribbon cable. The unused 8 pins are connected to capacitors on the OM13082 board (presumably for a different LCD display).
Here are the pins:
LCD12864 ribbon FPC-WKG12864... ST7565S controller OM13082 OM13082 LCD side external connector connector CCT ======== ======================= ========= ======= 1 CS 1 CS R8 -> CS 2 /RES 2 RST nRST 3 CD 3 C/D R11 -> CD 4 4 WR (NC) 5 5 RD (NC) 6 D0 6 D0 (NC) 7 D1 7 D1 (NC) 8 D2 8 D2 (NC) 9 D3 9 D3 (NC) 10 D4 10 D4 (NC) 11 D5 11 D5 (NC) 12 D6(SCL) 12 D6/SCK SCLK 13 D7(SI) 13 1 - 13 = thin wires D7/SID MOSI 14 VSS 14 Thick wire VSS GND 17 VOUT 15 VOUT C20 -> GND 16 NC CAP3P C14 17 NC CAP1N C14/C18 18 NC CAP1P C18 15 19 CAP2P C19 16 20 CAP2N C19 21 NC V4 C13 -> VDD 22 NC V3 C12 -> VDD 23 NC V2 C11 -> VDD 24 NC V1 C10 -> VDD 25 NC V0 C9 -> VDD 18 C86 26 L:C86/H:C68 VDD MPU interface. H = 6800 series. L = 8080. 19 P/S 27 L:S/H:P GND L = serial (SCL/SI) 20 28 Thick wire VDD VDD VDD
Hi, John,
Thanks, I see.
BR
Xiangjun Rong
Hi, John,
The OM13082 board uses LCD12864 as liquid screen, the LCD12864 liquid screen has the backlight pins exactly. The Pin 19 is LEDA pin(it should connect +5V of backlight) , the pin 20 is LEDK pin(it should connect to GND, the GND of back light).
This is the data sheet of LCD12864, but it is written with Chinese.
http://www.dfrobot.com.cn/image/data/FIT0021/CN/LCD12864%20chinese%20char.pdf
Regarding the board, I think the LEDA/LEDK should be connected to +5V rather than a capacitor.
BR
XiangJun Rong