NVT2008; NVT2010 unused channels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVT2008; NVT2010 unused channels

625件の閲覧回数
cdai
Contributor I

I don't need to use all the channels on the level translator NV2008. I don't see any connection guidelines for usused pins on the datasheet and was  wondering if there are any recommendations. Leave them floating? tie to ground?, etc

0 件の賞賛
返信
1 返信

576件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

There are several acceptable ways of dealing with unused channels and treating them as ‘not connected’ is probably the easiest. Alternatively, the unused channel pins can be connected together and tied to GND.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信