NVT2008; NVT2010 unused channels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVT2008; NVT2010 unused channels

626 Views
cdai
Contributor I

I don't need to use all the channels on the level translator NV2008. I don't see any connection guidelines for usused pins on the datasheet and was  wondering if there are any recommendations. Leave them floating? tie to ground?, etc

0 Kudos
Reply
1 Reply

577 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

There are several acceptable ways of dealing with unused channels and treating them as ‘not connected’ is probably the easiest. Alternatively, the unused channel pins can be connected together and tied to GND.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply