The NHS3152 IC has a sleep and deep sleep power savings modes. But no description as the reduction in power when these modes are enabled. Any guidance?
Solved! Go to Solution.
Hello @bmeyer ,
There is no detailed documentation on these power modes, the power gain compared to deep-power down is limited.
The difference between sleep and deep-sleep is only the handling of the EEPROM.
The power gain is dependent on the Sysclk frequency, as can be seen below in a graph of a typical application.
More power can be conserved by slowing down the Sysclk.
There is a slight increase of the Idd current (up to +12uA) when the Vdd voltage drops below 2.2V.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Kan:
Thanks for the guidance. However, this doc still only details current consumption during active and deep power down. Doesn't mention current consumption during sleep and deep sleep.
Hello @bmeyer ,
There is no detailed documentation on these power modes, the power gain compared to deep-power down is limited.
The difference between sleep and deep-sleep is only the handling of the EEPROM.
The power gain is dependent on the Sysclk frequency, as can be seen below in a graph of a typical application.
More power can be conserved by slowing down the Sysclk.
There is a slight increase of the Idd current (up to +12uA) when the Vdd voltage drops below 2.2V.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello @bmeyer ,
If you have download the SDK package for NHS3152, you may find the doc on this topic, please kindly refer to the following for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------