NHS3152 Sleep and deep sleep Power savings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3152 Sleep and deep sleep Power savings

Jump to solution
886 Views
bmeyer
Contributor II

The NHS3152 IC has a sleep and deep sleep power savings modes. But no description as the reduction in power when these modes are enabled. Any guidance?

0 Kudos
1 Solution
848 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @bmeyer ,

 

There is no detailed documentation on these power modes, the power gain compared to deep-power down is limited.
The difference between sleep and deep-sleep is only the handling of the EEPROM.

The power gain is dependent on the Sysclk frequency, as can be seen below in a graph of a typical application.
More power can be conserved by slowing down the Sysclk.

There is a slight increase of the Idd current (up to +12uA) when the Vdd voltage drops below 2.2V.

nhs low power mode.png

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
872 Views
bmeyer
Contributor II

Hello Kan:

Thanks for the guidance. However, this doc still only details current consumption during active and deep power down. Doesn't mention current consumption during sleep and deep sleep. 

0 Kudos
849 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @bmeyer ,

 

There is no detailed documentation on these power modes, the power gain compared to deep-power down is limited.
The difference between sleep and deep-sleep is only the handling of the EEPROM.

The power gain is dependent on the Sysclk frequency, as can be seen below in a graph of a typical application.
More power can be conserved by slowing down the Sysclk.

There is a slight increase of the Idd current (up to +12uA) when the Vdd voltage drops below 2.2V.

nhs low power mode.png

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

883 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @bmeyer ,

 

If you have download the SDK package for NHS3152, you may find the doc on this topic, please kindly refer to the following for details.

nhs low power modes.png

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos