MX27_FULL_VPU_SW_LINUX_REL3_BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX27_FULL_VPU_SW_LINUX_REL3_BSP

2,227 Views
gale
Contributor I
I can't download  MX27_FULL_VPU_SW_LINUX_REL3_BSP.
Someoen have download it ,please sent me,mail:gale320@gmail.com
Thanks!
0 Kudos
Reply
4 Replies

702 Views
gale
Contributor I
I have registered.Contact with them .Can't download it until now.

Some one have it ,send me,thanks!
0 Kudos
Reply

702 Views
fabio_estevam
NXP Employee
NXP Employee
Have you placed your Freescale's contact information? He/she should receive a link for the download and then pass it to you.
 
Regards,
 
Fabio Estevam
0 Kudos
Reply

702 Views
Michiel
Contributor I

I have the same problem and submitted a service request for it (1-576050160). The answer I got is that it has been removed because of the ITC order and will be restored whenever they are in a state in which they are compliant with the order.

This is really a bummer as I'm in a kind of hurry with a project. If someone could provide a link that would be great. (or send it to m_ettema@hotmail.com)

 

0 Kudos
Reply

702 Views
fabio_estevam
NXP Employee
NXP Employee
What is the error you get?
 
Have you registered to Freescale's website?
 
Regards,
 
Fabio Estevam
0 Kudos
Reply