MRFX1K80H, solder reflow or mechanical mounting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRFX1K80H, solder reflow or mechanical mounting

352 Views
dan-in-sd
Contributor I

Hello,

 

I would like the manufacturer (NXP)  to provide recommended practice for mounting the High Power LDMOS  MRFX1K80H devices:

 

1)   Use 'Liquid Metal' thermal grease and two M3 screws,   Torque screw to  {TBD}  torque value.

or

2)  Create a well in the copper heat spreader that just fits the LDMOS device,  apply a thin layer of solder paste on the bottom of device,  then place device in the well, and reflow solder 

    (what's recommended for reflow profile?   i.e. ramp to 240C,   then jump to 260C for 15s. then cool)

 

Which one is best practice for such a high power device?   Method   #1  or   # 2 

thanks

Dan

0 Kudos
Reply
1 Reply

332 Views
Alondra
NXP TechSupport
NXP TechSupport

Please see our guidelines for solder reflow mounting of high-power RF for MRFX1K80H 

 

Solder Reflow Attach Method for High Power RF Devices in Air Cavity Packages

https://www.nxp.com/docs/en/application-note/AN1908.pdf

Best regards

 

0 Kudos
Reply