MRF101AN - VHF oscillation issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MRF101AN - VHF oscillation issue

433 次查看
marco_uni
Contributor I

Hi, 

We are having issue with newly purchased MRF101AN-VHF kit. While the drain voltage is set to 50 V reading zero current, we started increasing gate voltage to 2.5 V, and noticed only 10 mA current at the drain. After increasing gate voltage slightly above 2.55V, we saw drain current jumps above 1.3 A. We had to shutdown everything since there is possibly defect on one of the components. Any idea what would be the cause of this issue?

 

Thanks,

Mark20231213_122201_01.jpg

 

20231213_120035.jpg

 

0 项奖励
回复
1 回复

411 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello, I will follow up on your ticket 00584923

0 项奖励
回复