已解决! 转到解答。
Medina,
Here's a thing to check if you haven't already done so.
All the GPIO 0-31 functions are multiplexed so you do have to make sure the pin isn't being used for another function.
Here are some excertps from the MPC8313 Engineering Reference Manual Rev. 1 07/2007 that may help
From section: 3.4 External Signal Description
From Table 3-6 External Signals—Detailed Signal Descriptions
Signal I/O Description: CFG_LBIU_MUX_EN (LA[0:15]/GPIO)
Pin type: Input Meaning:
Asserted—GPIO ports function according to the values in their configuration registers (this may be LBC or non-LBC functionality).
Negated—GPIO ports function as LA[0:15] irrespective of the value in their configuration registers.
Also see, 5.3.2.5 System I/O Configuration Register Low (SICRL). Bits 2-13 control if GPIO is enabled or other functions, see table in spec. The reset values of this register typically default to GPIO, but there may be software and/or board init that is setting this register to enable an alternate function rather than the GPIO you are trying to use. This register is read/write, so you can check it's current value by reading it.
Hope this helps :smileyhappy:
- abartky
Medina,
Here's a thing to check if you haven't already done so.
All the GPIO 0-31 functions are multiplexed so you do have to make sure the pin isn't being used for another function.
Here are some excertps from the MPC8313 Engineering Reference Manual Rev. 1 07/2007 that may help
From section: 3.4 External Signal Description
From Table 3-6 External Signals—Detailed Signal Descriptions
Signal I/O Description: CFG_LBIU_MUX_EN (LA[0:15]/GPIO)
Pin type: Input Meaning:
Asserted—GPIO ports function according to the values in their configuration registers (this may be LBC or non-LBC functionality).
Negated—GPIO ports function as LA[0:15] irrespective of the value in their configuration registers.
Also see, 5.3.2.5 System I/O Configuration Register Low (SICRL). Bits 2-13 control if GPIO is enabled or other functions, see table in spec. The reset values of this register typically default to GPIO, but there may be software and/or board init that is setting this register to enable an alternate function rather than the GPIO you are trying to use. This register is read/write, so you can check it's current value by reading it.
Hope this helps :smileyhappy:
- abartky