Hallo!
I am pretty new to this device and I struggle with understanding few things.
I would like to send a '1' (high) value to one of the pins. I can't get it done. Here is what I tried (with S32DS IDE).
1. Pin selection and intialisation:
I want to use PA1 in J3 area. I clicked on the 'pin_mux:PinSettings' in the components area and used the GUI to pick GPIO 1 from SIUL2 module. I set it to PA[1] and to 'Output'. After 'generating processer expert code' my pin_mux.c got updated with an entry for that pin. It reads that .pinPortIdx = 1u, and .gpioBase = PTA . Seems fine.
Next I entered this function in my main.c to initialise:
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
2. Sending 'High' to a pin:
Just underneath the pin initialisation line I called this function:
PINS_DRV_WritePin(PTA, 1u, 1);
Unfortunatelly this doesn't work. I mean that I can't measure any voltage on the pin, and I can't find any register entries that change when I debug the code.
My questions are:
1. How does the MPC574G use the embedded registers to send a 'high' on a pin? In the LED example from the nxp website, a mask was used that set only one bit in the fourth byte of a register to '1', which turned the onboard LED on. Does it mean that only specific bits of a register get transfered to a pin?
2. How can i figure out what are the connections between embedded registers and pins that are set up in 'PinSettings' GUI.
3. What can i do to make my code work?
thanks in advance for your help.
Here is my main() from main.c :
int main(void)
{
/* Write your local variable definition here */
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of Processor Expert internal initialization. ***/
/* Initialze pins */
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
/* send 'high' to pin*/
PINS_DRV_WritePin(PTA, 1u, 1);
/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
/*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
#ifdef PEX_RTOS_START
PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of RTOS startup code. ***/
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;;) {
if(exit_code != 0) {
break;
}
}
return exit_code;
/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/
已解决! 转到解答。
Hi,
your code looks normal, it should work.
1) first the SIUL2.MSCR[1] register should have OBE bit set and SSS field cleared to have PTA1 pin configured as GPIO output. You can refer to this register in debugger after PINS_DRV_Init is called.
Then the value is written into port using SIUL2.GPDOn or SIUL2.PGPDOn registers. Check in a debugger GPDO1 (GPDO0_3) or PGPDO0 register.
2) should be described in SIUL2 chapter of the RM
3) did you measure right pin? PTA1 is on J3.1 header.
Anyway you can try "hello_world_mpc5748g" demo example from S32 design studio. It toggles with a LED.
I tried to add PTA1 and output is working properly.
BR, Petr
Hi,
your code looks normal, it should work.
1) first the SIUL2.MSCR[1] register should have OBE bit set and SSS field cleared to have PTA1 pin configured as GPIO output. You can refer to this register in debugger after PINS_DRV_Init is called.
Then the value is written into port using SIUL2.GPDOn or SIUL2.PGPDOn registers. Check in a debugger GPDO1 (GPDO0_3) or PGPDO0 register.
2) should be described in SIUL2 chapter of the RM
3) did you measure right pin? PTA1 is on J3.1 header.
Anyway you can try "hello_world_mpc5748g" demo example from S32 design studio. It toggles with a LED.
I tried to add PTA1 and output is working properly.
BR, Petr