NCK2910 PLL Unlock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NCK2910 PLL Unlock

370 Views
1069466534
Contributor II

NCK2910 operates in RX ON mode, and when the ambient temperature ranges from 15 ℃ to 60 ℃, 2910 stops working and an RF Event occurs, type 0xF4-PLL Unlock. Currently, we have checked the external crystal oscillator and found that the PPM value is within the range. May I ask if there are any other possible situations that may cause PLL Unlock during temperature difference changes?

0 Kudos
Reply
0 Replies