MC33771C capacitve isolation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33771C capacitve isolation

跳至解决方案
795 次查看
Vladimir_A
Contributor I

Hello,

I see that new version of BMS AFE support capacitive isolation (table 1. https://www.nxp.com/docs/en/application-note/AN12633.pdf ). But, I can't find details about implementation. Application note AN12626 https://www.nxp.com/docs/en/application-note/AN12626.pdf describe TPL over transformer only.
Could you please provide me the requirements for the capacitors in case of capacitive isolation?

0 项奖励
回复
1 解答
649 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello, sorry for the delay in replaying. 

For capacitor selection, the voltage rate depends on the application/ The customer should select X7R or X7S dielectric for automotive temperature range. No need of specific low ESL/ESR.

Safety capacitors (soft termination from TDK), or two capacitors in series, should be considered for capacitors connected to high voltage and low impedance nets (batterry cells, TPL isolation, ...)

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
650 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello, sorry for the delay in replaying. 

For capacitor selection, the voltage rate depends on the application/ The customer should select X7R or X7S dielectric for automotive temperature range. No need of specific low ESL/ESR.

Safety capacitors (soft termination from TDK), or two capacitors in series, should be considered for capacitors connected to high voltage and low impedance nets (batterry cells, TPL isolation, ...)

Hope this helps.

0 项奖励
回复
772 次查看
Vladimir_A
Contributor I

Hi Erika, thank you for the answer.
I just checked this part of documentation and see that there are only high level requirements are provide - capacitance, resistance and voltage of ESD. One characteristics for each component.
I think that the type, class, voltage of capacitor should determined at least. Maybe some type of frequecy characteristics. Due to high frequency and high voltage operation bad choice of capacitor and ESD may affect on the result.

0 项奖励
回复
778 次查看
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The requirements for the capacitors in case of capacitive isolation are described in the MC33771C datasheet, please refer to section 13.

Hope this helps.

0 项奖励
回复