MC33771C capacitve isolation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C capacitve isolation

Jump to solution
577 Views
Vladimir_A
Contributor I

Hello,

I see that new version of BMS AFE support capacitive isolation (table 1. https://www.nxp.com/docs/en/application-note/AN12633.pdf ). But, I can't find details about implementation. Application note AN12626 https://www.nxp.com/docs/en/application-note/AN12626.pdf describe TPL over transformer only.
Could you please provide me the requirements for the capacitors in case of capacitive isolation?

0 Kudos
Reply
1 Solution
431 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, sorry for the delay in replaying. 

For capacitor selection, the voltage rate depends on the application/ The customer should select X7R or X7S dielectric for automotive temperature range. No need of specific low ESL/ESR.

Safety capacitors (soft termination from TDK), or two capacitors in series, should be considered for capacitors connected to high voltage and low impedance nets (batterry cells, TPL isolation, ...)

Hope this helps.

View solution in original post

0 Kudos
Reply
3 Replies
432 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, sorry for the delay in replaying. 

For capacitor selection, the voltage rate depends on the application/ The customer should select X7R or X7S dielectric for automotive temperature range. No need of specific low ESL/ESR.

Safety capacitors (soft termination from TDK), or two capacitors in series, should be considered for capacitors connected to high voltage and low impedance nets (batterry cells, TPL isolation, ...)

Hope this helps.

0 Kudos
Reply
554 Views
Vladimir_A
Contributor I

Hi Erika, thank you for the answer.
I just checked this part of documentation and see that there are only high level requirements are provide - capacitance, resistance and voltage of ESD. One characteristics for each component.
I think that the type, class, voltage of capacitor should determined at least. Maybe some type of frequecy characteristics. Due to high frequency and high voltage operation bad choice of capacitor and ESD may affect on the result.

0 Kudos
Reply
560 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The requirements for the capacitors in case of capacitive isolation are described in the MC33771C datasheet, please refer to section 13.

Hope this helps.

0 Kudos
Reply