MC33665 compatible with MC33771x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33665 compatible with MC33771x

728件の閲覧回数
Patrick_Pavle
Contributor III

Hello Community,

is the transceiver MC33665 compatible with MC33771B or only with MC33771C, MC33772C, and MC33775A?

best regards

Patrick

0 件の賞賛
返信
5 返答(返信)

706件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Patrick_Pavle,

I hope all is great with you. Thank you for using the NXP communities.

Because of the TPL version, the MC33771B is not compatible.

The MC33665A is compatible with TPL2 (MC33771C, MC33772C) and TPL3 (MC33775A, MC33774A) BCCs only.

I hope this information helps.

Regards,

David

0 件の賞賛
返信

696件の閲覧回数
Patrick_Pavle
Contributor III

Hello @diazmarin09,

but why is MC33664 compatible with TP1 (MC33771B) and TP2 (MC33771C)? 

Regards,

Patrick

0 件の賞賛
返信

688件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Patrick_Pavle,

Thank you for using the NXP community.

I do recommend the following application note:

AN12626 - MC33771x/MC33772x transformer and wire guide on the TPL network

Both series are battery communication ICs with different features. If you need to work with the MC33771B, I highly recommend considering the MC33664 device.

I hope this information helps.

Regards,

David

0 件の賞賛
返信

656件の閲覧回数
Patrick_Pavle
Contributor III

Hello @diazmarin09 

thanks for responding!

I don´t unterstand why MC33664 is compatible with TPL1 and TPL2, but MC33665 is not compatible with TPL1? 

best regars,

Patrick

0 件の賞賛
返信

702件の閲覧回数
Patrick_Pavle
Contributor III

Hello @diazmarin09 ,

thanks for responding! 

Do you have links or data sheets, where I can see the differences between the TPL versions? 

Regards,

Patrick

0 件の賞賛
返信