MC33665 compatible with MC33771x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33665 compatible with MC33771x

520 Views
Patrick_Pavle
Contributor III

Hello Community,

is the transceiver MC33665 compatible with MC33771B or only with MC33771C, MC33772C, and MC33775A?

best regards

Patrick

0 Kudos
Reply
5 Replies

498 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Patrick_Pavle,

I hope all is great with you. Thank you for using the NXP communities.

Because of the TPL version, the MC33771B is not compatible.

The MC33665A is compatible with TPL2 (MC33771C, MC33772C) and TPL3 (MC33775A, MC33774A) BCCs only.

I hope this information helps.

Regards,

David

0 Kudos
Reply

488 Views
Patrick_Pavle
Contributor III

Hello @diazmarin09,

but why is MC33664 compatible with TP1 (MC33771B) and TP2 (MC33771C)? 

Regards,

Patrick

0 Kudos
Reply

480 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Patrick_Pavle,

Thank you for using the NXP community.

I do recommend the following application note:

AN12626 - MC33771x/MC33772x transformer and wire guide on the TPL network

Both series are battery communication ICs with different features. If you need to work with the MC33771B, I highly recommend considering the MC33664 device.

I hope this information helps.

Regards,

David

0 Kudos
Reply

448 Views
Patrick_Pavle
Contributor III

Hello @diazmarin09 

thanks for responding!

I don´t unterstand why MC33664 is compatible with TPL1 and TPL2, but MC33665 is not compatible with TPL1? 

best regars,

Patrick

0 Kudos
Reply

494 Views
Patrick_Pavle
Contributor III

Hello @diazmarin09 ,

thanks for responding! 

Do you have links or data sheets, where I can see the differences between the TPL versions? 

Regards,

Patrick

0 Kudos
Reply