Hello Community,
is the transceiver MC33665 compatible with MC33771B or only with MC33771C, MC33772C, and MC33775A?
best regards
Patrick
Hello Patrick_Pavle,
I hope all is great with you. Thank you for using the NXP communities.
Because of the TPL version, the MC33771B is not compatible.
The MC33665A is compatible with TPL2 (MC33771C, MC33772C) and TPL3 (MC33775A, MC33774A) BCCs only.
I hope this information helps.
Regards,
David
Hello @diazmarin09,
but why is MC33664 compatible with TP1 (MC33771B) and TP2 (MC33771C)?
Regards,
Patrick
Hello Patrick_Pavle,
Thank you for using the NXP community.
I do recommend the following application note:
AN12626 - MC33771x/MC33772x transformer and wire guide on the TPL network
Both series are battery communication ICs with different features. If you need to work with the MC33771B, I highly recommend considering the MC33664 device.
I hope this information helps.
Regards,
David
Hello @diazmarin09
thanks for responding!
I don´t unterstand why MC33664 is compatible with TPL1 and TPL2, but MC33665 is not compatible with TPL1?
best regars,
Patrick
Hello @diazmarin09 ,
thanks for responding!
Do you have links or data sheets, where I can see the differences between the TPL versions?
Regards,
Patrick