MC10XS4200 current level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC10XS4200 current level

Jump to solution
545 Views
mertsahin
Contributor II

Hi,

 

We would like to drive 27 V motor which has continuous current 6 A and instantaneous current 30 A for 2 seconds.

1) Can this part handle it? If not should I use 6 mohm version? 

2) Is it possible to parallel multipke MC10XS4200 devices to obtain more current?

3) If not 2 seconds possible then how many ms can this device withstand to 30 A ins. current?

 

Thanks a lot.

0 Kudos
Reply
1 Solution
537 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mert,

The MC10XS4200 cannot drive 30A for 2 seconds, you can find the timing as below.

The max. timing is 350ms when motor current goes up. Even in parallel, current can be doubled, but time is fixed.

You can use the MC06XS4200 due to DC current up to 15A, use two outputs in parallel, then current is also doubled to 30A.

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

View solution in original post

2 Replies
538 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mert,

The MC10XS4200 cannot drive 30A for 2 seconds, you can find the timing as below.

The max. timing is 350ms when motor current goes up. Even in parallel, current can be doubled, but time is fixed.

You can use the MC06XS4200 due to DC current up to 15A, use two outputs in parallel, then current is also doubled to 30A.

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

512 Views
mertsahin
Contributor II
Tomas, thanks a lot for your speedy response
0 Kudos
Reply