LS1028A JTAG Connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A JTAG Connectivity

1,116 Views
Sathian
Contributor II

We have custom based LS1028A board and trying to halt the processor via JTAG. 

We could able to do "halt" in EVM(Attached image) but not in custom board, What could be the problem and solution ?

0 Kudos
1 Reply

1,109 Views
ufedor
NXP Employee
NXP Employee

Which exactly DUT board is in question?

Is POR behaviour of the reset signals on the DUT board similar to shown in the "Figure 6. Power-On Reset Sequence" in the QorIQ LS1028A Reference Manual?

Is the DUT board capable to boot?

Please confirm that JTAG interface is implemented as described in the AN12028 - QorIQ LS1028A Design Checklist, 5.20 JTAG pin termination recommendations.

Is TRST_B asserted during power-on reset flow?

 

0 Kudos