Hello All,
I'm currently working on LS1021A - TWR Board. We have Successfully loaded the QUICC Firmware please find the below logs for your reference.
"Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1"
I included the qe_ic driver and UCC Uart driver into the kernel. I got below logs for the successful loading of UCC uart driver.
[ 1.955532] Freescale QUICC Engine UART device driver
[ 1.961056] 2402000.ucc: ttyQE0 at MMIO 0x2402000 (irq = 38, base_baud = 9375000) is a QE
[ 1.969579] ucc_uart 2402000.ucc: UCC1 assigned to /dev/ttyQE0
[ 1.975734] 2402200.ucc: ttyQE1 at MMIO 0x2402200 (irq = 39, base_baud = 9375000) is a QE
[ 1.984191] ucc_uart 2402200.ucc: UCC3 assigned to /dev/ttyQE1
Once i get the console i check the interrupt entry of QUICC driver using the below command "cat /proc/interrupts"
Find the below attachment "interrupts.txt".
Please let me know whether I need to get the interrupt entry in the "/proc/interrupts". And also I'm running the below commands for transmitting the data through ttyQE0 by using the below command.
echo "hi" > /dev/ttyQE0
Here I want to check whether I got transmitted the interrupt or not. Can you please help me to check it.
For your reference "TWR-LS1021A-kernel-logs.txt" attached below.
Thanks in Advance.
已解决! 转到解答。
Verification in Linux
1. After uboot startup,set "qe" parameter in hwconfig.
2. After bootup kernel, create the device node manually:
QE serial port1: mknod /dev/ttyQE0 c 204 46
QE serial port2: mknod /dev/ttyQE1 c 204 47
3. Type the command: getty 115200 /dev/ttyQE0
4. Connect one console cable(RS485 to RS232)to PC COM2 and open a terminal binding with it, and Set the terminal baud rate to 115200.
5. You can type any shell command in UCC UART TERMINAL.
Verification in Linux
1. After uboot startup,set "qe" parameter in hwconfig.
2. After bootup kernel, create the device node manually:
QE serial port1: mknod /dev/ttyQE0 c 204 46
QE serial port2: mknod /dev/ttyQE1 c 204 47
3. Type the command: getty 115200 /dev/ttyQE0
4. Connect one console cable(RS485 to RS232)to PC COM2 and open a terminal binding with it, and Set the terminal baud rate to 115200.
5. You can type any shell command in UCC UART TERMINAL.
1. After running the microcom command, we are getting the QUICC interrupt entry in cat /proc/interrupts.
Command: microcom -s 115200 /dev/ttyQE0
log :
~# cat /proc/interrupts
CPU0 CPU1
16: 0 0 GIC 29 Edge arch_timer
17: 956 781 GIC 30 Edge arch_timer
18: 0 0 GIC 27 Edge kvm guest timer
22: 0 0 GIC 25 Edge vgic
25: 0 0 GIC 107 Level SCM_IRQ
26: 6957 0 GIC 126 Level mmc0
29: 0 0 GIC 129 Level 2110000.dspi
30: 87 0 GIC 120 Level 2180000.i2c
31: 0 0 GIC 121 Level 2190000.i2c
32: 292 0 GIC 118 Level serial
40: 0 0 GIC 150 Level 29d0000.ftm0
41: 0 0 GIC 147 Level 2ad0000.watchdog
43: 0 0 GIC 167 Level eDMA
47: 0 0 GIC 205 Level gianfar_ptp
51: 0 0 GIC 125 Level xhci-hcd:usb1
56: 0 0 QEIC 32 Level ucc-uart
57: 9 0 GIC 176 Level eth0_g0_tx
58: 133 0 GIC 177 Level eth0_g0_rx
59: 0 0 GIC 178 Level eth0_g0_er
60: 52 0 GIC 179 Level eth0_g1_tx
61: 0 0 GIC 180 Level eth0_g1_rx
62: 0 0 GIC 181 Level eth0_g1_er
IPI0: 0 0 CPU wakeup interrupts
IPI1: 0 0 Timer broadcast interrupts
IPI2: 1695 1349 Rescheduling interrupts
IPI3: 0 0 Function call interrupts
IPI4: 2 13 Single function call interrupts
IPI5: 0 0 CPU stop interrupts
IPI6: 1 0 IRQ work interrupts
IPI7: 0 0 completion interrupts
2. When I transmit data through microcom, the UCC_uart interrupt is not getting triggered.
3.We suspect that the QUICC interrupt controller is enabled in the GIC (interrupt number - 141). We need the procedure to enable the GIC interrupt (interrupt number - 141).
Can you please help me to check it.
For your reference "TWR-LS1021A-kernel-logs.txt" and "interrupts.txt" attached below.
Continue to discuss in
https://community.nxp.com/t5/Other-NXP-Products/QUICC-ENGINE-VALlDATION/td-p/1894128