Is there a suitable replacement for BGA2709?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a suitable replacement for BGA2709?

1,396 Views
1318910567
Contributor I

只需测试而不是bga 2709频谱测试可以接收数字dvb-tno。

Test PCB's waveform on frequency spectrum OK Connect antenna to receive signal not OK

The voltage was adjusted to 2.6v and was barely received.微信图片_20191226091520.jpg

0 Kudos
Reply
4 Replies

1,159 Views
1318910567
Contributor I

接收频率  40-790mhz 是要选择2869还是2874比较好微信图片_20191230134335.jpg

0 Kudos
Reply

1,159 Views
LPP
NXP Employee
NXP Employee

BGA2709 is no longer manufactured. You should not use it for a new design.
BGA2709 has been characterized to work at 5V supply.
2.6V is out of recommended range.

BGA2869 has better dynamic range (IIP3) than BGA2874.
But, for 2.5V operation, you should use BGA2874 whereas BGA2869 is suitable for 5V.

Have a great day,

Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

907 Views
Frank1963
Contributor I

who is the correspondent of the bga 2709? I have trouble finding it.

0 Kudos
Reply

1,159 Views
1318910567
Contributor I

pcb安装bga2709正常接收的,2869电压调到2.6v  勉强接收

0 Kudos
Reply