Is there a compatible driver for the PCA9685 led driver with Linux kernel 4.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a compatible driver for the PCA9685 led driver with Linux kernel 4.1?

808 Views
jochem_van_boxt
Contributor I

I am working on an embedded product, for which we're looking to use the PCA9685 led driver chip. The product uses a Yocto built Linux kernel on version 4.1. There is a a driver for the PCA9685 in the current master branch of the Linux kernel source, but not in version 4.1. Will the driver from the master branch be compatible with 4.1? If not, is there a driver that is compatible?

0 Kudos
Reply
1 Reply

712 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately there are no Linux drivers for the PCA8565, if useful, there is an un-official code example in the NXP communities in the following link: https://community.nxp.com/docs/DOC-331808

 

Download the zip file and inside the src folder, you can find the PCA8565.c and PCA8565.h files.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply