Inline assembly - PowerPC - return value override

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inline assembly - PowerPC - return value override

1,372 Views
Ido100
Contributor I

Hello community!

I want to create some inline assembly examples for PowerPC architecture.
During the implementation I encountered several challenges.

For Example:

Function that sum two local variables and return the sum value.

While debugging the code I found out the code save the correct sum value in r0 register, but before it return value, I saw the r3 override with 0 value.  

 

int my_asm_add_local(void)
{
    int sum = 0;
    int a = 4, b = 2;

    asm volatile("se_add %1, %2\n\t"
                 "se_stw %1, 0(%0)\n\t"
                 : "=r" (sum)
                 : "r" (a), "r" (b)
    );

    return sum;
}

 

code from debugger

 

int my_asm_add_local(void)
182106F0  my_asm_a.:e_stwu    r1,-0x10(r1)   ; r1,-16(r1)
0080                se_mflr   r0
D501                se_stw    r0,0x14(r1)    ; a,20(r1)
{
    int sum = 0;
    int a = 4, b = 2;
4840                se_li     r0,0x4         ; a,4
4823                se_li     r3,0x2         ; r3,2

    asm volatile("se_add %1, %2\n\t"
0430                se_add    r0,r3          ; a,b
D003                se_stw    r0,0x0(r3)     ; a,0(r3)
                 "se_stw %1, 0(%0)\n\t"
                 : "=r" (sum)
                 : "r" (a), "r" (b)
    );

    return sum;
4803                se_li     r3,0x0         ; b,0
}
C501                se_lwz    r0,0x14(r1)    ; a,20(r1)
0090                se_mtlr   r0
20F1                se_addi   r1,0x10        ; r1,16
0004                se_blr
4444                se_or     r4,r4

 


 I would appreciate any help.

In addition, if anyone knows a good source information with examples of inline assembly for PowerPC, it is could be help.

0 Kudos
Reply
1 Reply

1,265 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please disassemble the library code provided in CodeWarrior project to generate assembly code.

0 Kudos
Reply