Hi, Please provide source and load impedance details at 108Mhz to 138Mhz frequency range for MRF6V2150NR1
We have no measured data at these frequencies.
Input and load impedances simulated with MRF6V2150NR1 ADS model.
Optimized for best PAE or P1dB power at 1dB output compression.
maximum Power
Input Load
108 3.49-j11.05 3.65+j2.32
138 2.67-j9.33 3.65+j2.32
maximum PAE
Input Load
108 3.41-j10.4 4.67+j4.82
138 2.52-j9.02 3.32+j3.89
Have a great day,
Pavel
NXP TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------