Hi, Please provide source and load impedance details at 108Mhz to 138Mhz frequency range for MRF6V2150NR1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, Please provide source and load impedance details at 108Mhz to 138Mhz frequency range for MRF6V2150NR1

679 Views
ajivs
Contributor I

Hi, Please provide source and load impedance details at  108Mhz  to 138Mhz frequency range for MRF6V2150NR1

0 Kudos
Reply
2 Replies

584 Views
LPP
NXP Employee
NXP Employee

We have no measured data at these frequencies.

Input and load impedances simulated with MRF6V2150NR1 ADS model.

Optimized for best PAE or P1dB power at 1dB output compression.

maximum Power
    Input        Load
108    3.49-j11.05    3.65+j2.32
138    2.67-j9.33    3.65+j2.32

maximum PAE
    Input        Load
108    3.41-j10.4    4.67+j4.82
138    2.52-j9.02    3.32+j3.89

Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

584 Views
ajivs
Contributor I

Hi

Thanks for the feedback. However I am unable to download ADS Model for this part. "Page Not Found" window appears after clicking download button.

Please share this data.

Regards

Aji

0 Kudos
Reply