hello, I have a problem for a few days that I don't know how to solve. I have a project developed with FreeMaster 2.5, this project contains some pointers and some arrays, which are recognized by showing the address. However, if I open the project with FreeMaster 3.1 when I open the project it gives me some errors and the pointers and arrays are no longer found, how can I solve the problem?
hello, thanks for the reply I am forwarding you the photo of the freemaster version I am using (3.1.2.4) and I am forwarding you the photo of the freemaster version I used before (2.5.13.0).
in version 2.5.13.0 the address of the variable "theprogram.line [0] +0" was found without any kind of problem
if now I open the project (saved in .pmpx) with version 3.1.2.4, it happens that it is no longer able to retrieve the address of this array variable.
how can I do that the entire project opened with version 3.1.2.4 automatically finds all the addresses of the variables?
N.B the .elf file and the project are the same both when they are opened with one version and when they are opened with the other version
Hi,
If you reload the application project *.elf as the following Fig, then re-check the variable address, can you see the variable?
BR
XiangJun Rong
yes, I reloaded the .elf file, and in fact some variables I can open and find the address (with freemaster 3.1.2.4), two-dimensional arrays and pointers however that with freemaster 2.5 did not give problems now with freemaster 3.1. 2.4 the address is not found.
What's the chip part number?
hello, did you by any chance understand what my problem is?
hello thanks for the answer I found this problem with "MC56F84452VLH 96k 60Mhz"
@mich28 ,
Thank you for contacting NXP Technical support.
To provide you with better support, can you please let us know the part number you are using?