FS26 SBC init delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 SBC init delay

Jump to solution
2,110 Views
kjy106906
Contributor IV

Hello

I have a question regarding the FS26 SBC.

Is more delay needed in the following situations?
Standby -> SPI wake up -> delay 1.5ms -> SBC init

For 1.5ms, I referred to the phrase below in the datasheet.

SPI chip select wake-up:
– When the SPI wake up is enabled, the device wakes up with any activity on the SPI bus (transition from high to low of CSB pin).
– In case of a SPI wake up, the first SPI command is ignored, and the FS26 will be ableto respond to the subsequent SPI commands after 1.5 ms.

However, init fails with 1.5ms.
Init succeeds with 10ms.

Is there an exact delay guide?

0 Kudos
Reply
1 Solution
2,078 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1693985814828.png

Set this time above 7ms.

 

View solution in original post

0 Kudos
Reply
9 Replies
2,090 Views
guoweisun
NXP TechSupport
NXP TechSupport

No fully understand you wrote:

 init fails with 1.5ms.
Init succeeds with 10ms.

Could you please give more explain?

 

0 Kudos
Reply
2,080 Views
kjy106906
Contributor IV

Yes.

Standby -> SPI wake up -> delay 1.5ms -> Sbc_fs26_Init

-> return Not Ok

Standby -> SPI wake up -> delay 10ms -> Sbc_fs26_Init

-> return Ok

 

Tags (1)
0 Kudos
Reply
2,079 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1693985814828.png

Set this time above 7ms.

 

0 Kudos
Reply
2,019 Views
kjy106906
Contributor IV

@guoweisun 

SBC Standby -> SPI wake up -> delay 1.5ms -> Sbc_fs26_Init

-> return Not Ok

SBC Standby -> SPI wake up -> delay 10ms -> Sbc_fs26_Init

-> return Ok

I don't know why you are talking about RSTB time.
If I put the SBC in Standby, the SBC will not become a POR.
When MCU do SBC SPI wakeup, RSTB has already been released.

 

0 Kudos
Reply
2,012 Views
guoweisun
NXP TechSupport
NXP TechSupport

---

I don't know why you are talking about RSTB time.
If I put the SBC in Standby, the SBC will not become a POR.
When MCU do SBC SPI wakeup, RSTB has already been released.

---

After wake up SBC state machine still follow below, detail in datasheet page25:

guoweisun_0-1694074353834.png

 

0 Kudos
Reply
2,002 Views
kjy106906
Contributor IV

Yes.

It says "but maintained high during wake up from Standby" on it.

so 

SBC Standby (RSTB High) -> SPI wake up (RSTB High)-> delay 1.5ms (RSTB high) -> Sbc_fs26_Init(RSTB high) -> return Not Ok

RSTB is always high, so why is RSTB Release time and delay related?

Thank you

0 Kudos
Reply
1,946 Views
guoweisun
NXP TechSupport
NXP TechSupport

Although RSTB is high but the state machine still follow:

Default FS_OTP Loading->LBIST DONE->ENABLE Monitoring->ABIST1 test->enter INIT FS 

0 Kudos
Reply
1,915 Views
kjy106906
Contributor IV

Very Thank you I understood

0 Kudos
Reply
2,085 Views
guoweisun
NXP TechSupport
NXP TechSupport

I think below process:

Standby -> SPI wake up -> delay 1.5ms at same time the fail safety mechanism continue to flow as below picture if no failure will stop in INIT phase  -> SBC init

 

guoweisun_0-1693984140150.png

guoweisun_1-1693984180415.png

guoweisun_2-1693984196756.png

 

0 Kudos
Reply