my computer can't install EBTresos(EBtresosStudio_EBtresosStudio) tool, how to fix it.
Hi , Does this issue Resolved ? I also has the same problem
Can anyone help me with this issue?
Hi,
I've just tried to download in another PC, and similar to your situation, all downloaded files have the extension as *.gz. It led to setup.exe couldn't find the packages
After changed extension to *.uip, setup.exe could find the packages and could be opened.
So please note that you have to CHANGE the extension of the downloaded files, not UNZIP them.
Hi,
Please copy all the *.uip files, which are the necessary packages for EB installer, into another empty folder, as below:
Hints: choose show the extension of file in Folder options, to make sure you get the correct files
After that, try to run setup.exe.
I follow your proposal(copy all files to another empty folder), still have the same issue. compare to your file, I don't have EBtresosStudio_WibuKeyRuntime.uip .txt. from the website, i get package of EBtresosStudio_WibuKeyRuntime, after uncompress, i just can get the following two folder. i can't download Update-ACG-8.5_Studio-24.0.1-B192974_ImportantNotes directly, but i can copy the content to TXT file.
Hello,
Here is the required system environment of EB Tresos 24.0.1:
Please check your type of Windows (32-bit and 64-bit) to see if EB Tresos 24.0.1 can compatible with.
All of the environment is fulfilled, Is there another EB Tresos studio version to have a try.
My computer is Window 7 Professional Service Pack 1 64-bit, Processor is Quad-core, RAM is 16GB.
I realized that your file name seems not like the installer which is downloaded from www.nxp.com. Please check and re-download all of these files (if anything is missing)
I re-download all of these files. and first install setup.exe, there is a warning.
Hi,
Seems like it's a Windows compatible problem. Could you tell me which version of EB tresos you want to install? And please share the Windows version and your computer's specification.
1. AUTOSAR Tresos Studio 24.0.1
2. Window 7 Professional Service Pack 1, Intel(R) Xeon(R) CPU E5-1620 v3 @ 3.5GHz.
1. AUTOSAR Tresos Studio 24.0.1.
2. Windows 7 Professional Service Pack 1, Intel(R) CPU E5-1620 v3 @3.5GHz.