Driver for ADV7280A in Linux Environment (IMX6U)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for ADV7280A in Linux Environment (IMX6U)

1,829 Views
micro_tang
Contributor I

We chose an ADV7280A chip on the platform of IMX6,application of CVBS Camera in Linux Environment,but we couldn't find the corresponding driver. We need your help to provide it, TKS a lot!

PS:We checked some drive codes of ADV7182 that were circulated on the Internet and found that they were not available. At present, the camera is working , crystal also is working, but the image can't be obtained.

0 Kudos
Reply
6 Replies

1,620 Views
l_bruni
Contributor II

Dear Micro Tang, we've successfully used the driver for adv7180.c with some changes on the init register settings.

Regards,

Luca

0 Kudos
Reply

1,620 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello micro,

      I have ADV7282m driver for linux,  the driver is designed on older linux version, probably you will have to do a little change for your application, at least, it can help you check if the configurations of registers are correct.

I will send it to your personal email. check it , please!

Have a nice day!

BR,

Weidong

0 Kudos
Reply

1,620 Views
liyu1
Contributor III

请问您能发一份给我吗?ADV7282M的驱动,不胜感激!主要想参考一下寄存器配置,谢谢

0 Kudos
Reply

1,620 Views
micro_tang
Contributor I

我们也没有这颗的,抱歉啊

发自我的iPhone

在 2019年11月25日,下午9:23,liyu <admin@community.nxp.com> 写道:

NXP Community

Re: Driver for ADV7280A in Linux Environment (IMX6U)

reply from li yu in Other NXP Products - View the full discussion

请问您能发一份给我吗?ADV7282M的驱动,不胜感激!主要想参考一下寄存器配置,谢谢

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Other NXP Products by email or at NXP Community

Following Re: Driver for ADV7280A in Linux Environment (IMX6U) in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

>

0 Kudos
Reply

1,619 Views
micro_tang
Contributor I
Dear Wigros,
         Do you have any driver code for BT656 mode? Will MIPI and CVBS register configurations be different?
 
          PS: CSICR18[0,1]any users for debug, datasheet no description.
0 Kudos
Reply

1,619 Views
l_bruni
Contributor II

Hi Micro Tang, have you succeeded in doing ADV7280A working under Linux?

I'm trying the same thing with Android Oreo 8 and mx6q.

Kind regards,

Luca

0 Kudos
Reply