Could you tell me the thickness of the gold (Au) plating on the leads that solder to the PWB for part # MMRF1312HSR5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could you tell me the thickness of the gold (Au) plating on the leads that solder to the PWB for part # MMRF1312HSR5

870 Views
componentengine
Contributor I

Could you tell me the thickness of the gold (Au) plating on the leads that solder to the PWB for part # MMRF1312HSR5

Labels (1)
  • RF

0 Kudos
Reply
2 Replies

769 Views
LPP
NXP Employee
NXP Employee

This device has lead frame plating 30-50 uinches, flange plating 100 uinches of electrolytic gold over 100 uinches Ni-Co.


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

769 Views
componentengine
Contributor I

Thank you very much for the information

Heike Althaus

0 Kudos
Reply