Cannot taken branch to measure code coverage on S32R294

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot taken branch to measure code coverage on S32R294

1,290 Views
sonvungoc
NXP Employee
NXP Employee

Hi,

I am measure code coverage for some APIs relative ternary operator. Saw debugger cannot recognize branch when ternary operators are used and missing e_b also. It gives bad results measure code coverage. Please help me check it. My debugger as below:

  • Function not taken decision:

 

  • Function foo1 not taken decisionFunction foo1 not taken decisionFunction foo2 not taken decisionFunction foo2 not taken decisionFunction foo4 not taken decisionFunction foo4 not taken decisionFunction foo5 not taken decisionFunction foo5 not taken decisionFunction foo5 not taken decisionFunction foo5 not taken decision
  • Funtion taken decision:

        Funtion foo3 taken decisionFuntion foo3 taken decision

My code test as below:

 

///  typedefs to fix MISRA DIR4.6
typedef uint8_t BOOL;
#define TRUE ((uint8_t)1u)
#define FALSE ((uint8_t)0u)

typedef uint32_t FOO_ERRCODE;

#define FOO_ERR_NOERROR                  (0u)
#define FOO_ERR_INPUTOUTOFRANGE          (0x50001u)
#define FOO_ERR_INPUTOUTOFRANGE_2        (0x1u)

uint8_t foo1(uint8_t input1);
BOOL foo2(BOOL input2);
FOO_ERRCODE foo3(uint32_t input3);
FOO_ERRCODE foo4(uint32_t input4);
FOO_ERRCODE foo5(float32_t SeqInterval);

uint8_t foo1(uint8_t input1)
{
    uint8_t output1 = 0u;

    output1 = (input1 == 1u) ? 0u : 1u;

    return output1;
}

BOOL foo2(BOOL input2)
{
    BOOL output2 = FALSE;

    output2 = (input2 == TRUE) ? FALSE : TRUE;

    return output2;
}

FOO_ERRCODE foo3(uint32_t input3)
{
    FOO_ERRCODE errodeCode = FOO_ERR_NOERROR;

    errodeCode = (input3 > 32) ? FOO_ERR_NOERROR : FOO_ERR_INPUTOUTOFRANGE;

    return errodeCode;
}

FOO_ERRCODE foo4(uint32_t input4)
{
    FOO_ERRCODE errodeCode = FOO_ERR_NOERROR;

    errodeCode = (input4 > 32) ? FOO_ERR_NOERROR : FOO_ERR_INPUTOUTOFRANGE_2;

    return errodeCode;
}

FOO_ERRCODE foo5(float32_t SeqInterval)
{
    FOO_ERRCODE errodeCode = FOO_ERR_NOERROR;
    uint64_t tmpSeqInterval;

    tmpSeqInterval = (uint64_t)lroundf(SeqInterval * 1000.0f / 25.0f);
    if ((tmpSeqInterval >= 1u) && (tmpSeqInterval < 0xFFFFFFFFu))
    {
        errodeCode = FOO_ERR_NOERROR;
    }
    else
    {
        errodeCode = FOO_ERR_INPUTOUTOFRANGE;
    }

    return errodeCode;
}

void main(void)
{
    foo1(1u);
    foo1(0u);

    foo2(TRUE);
    foo2(FALSE);

    foo3(35u);
    foo3(25u);

    foo4(35u);
    foo4(25u);

    foo5(10u);
    foo5(0u);
    foo5(0xFFFFFFFFu);
}

 

My tool and enviroment:

  • Compiler Versions: 
     GNU Compiler Collection - GCC Version 4.9.4 20160726
 
  • SW Version:
- S32 Design Studio, version 2.1, Build ID 190624 with S32R294 development package version 2.1.0
- Lauterbach Trace32 PowerView for PowerPC, Version N.2021.06.000136240
 
  • HW Version:
- EVB S32R294RRU2 

 

0 Kudos
Reply
6 Replies

1,249 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not sure what is the issue here.

Saw debugger cannot recognize branch when ternary operators are used and missing e_b also.

Nor I see missing branch operation in your post. Is this issue with the translation or debugger processing?

Could you explain it in more detail?

Best regards,

Peter

0 Kudos
Reply

1,175 Views
sonvungoc
NXP Employee
NXP Employee

Hi Peter,

In my driver have a lot of ternary operator are used, I am trying cover all ternary operator, almost them are taken 100% coverage report by TRACE32. Some ternary operator cannot taken, I sure I have unit test for cover them, but TRACE32 reported improper. Actually, I don't know root cause issue yet.
I checked assembly code by debug TRACE32. Saw ternary operator are not taken 100% coverage have not command "e_b". Checked in ternary operator taken 100%, saw all of them have command "e_b".
I guess TRACE32 need command ""e_b" to measure code coverage.

assemblyFoo3 - Copy.PNG

Tags (1)
0 Kudos
Reply

1,157 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

what comes to my mind, is compiler translation.

Try to play with compiler optimizations, like no optimization at all , etc...

Debugger really displays only what is translated.

Also check output files form compilation to see if the translation corresponds with what you expect.

Best regards,

Peter

0 Kudos
Reply

1,273 Views
rweiss
Contributor V

For questions about TRACE32 please contact Lauterbach at https://support.lauterbach.com/

0 Kudos
Reply

1,171 Views
sonvungoc
NXP Employee
NXP Employee

Hi Reinhard,

I raised to Lauterbach team. But this issue still resolved yet

Tags (1)
0 Kudos
Reply

1,097 Views
rweiss
Contributor V

Please write to Lauterbach again and include a link to this thread, so we can combine your requests.

Regards,
Reinhard

0 Kudos
Reply