Tried to access the PCIe device on two s32v234 boards, unsuccessfully.
In U-Boot, pci commands, such as enum, get a "pci_bus_to_hose() failed" message.
With Lauterbach, tried accessing the PCIe section in its built-in register mechanism, and also accessing directly the address stated in the Reference Manual (0x72000000 - 0x72ffffff). In both cases I get a debug port time out error.
Does U-Boot not clock the PCIe bus on this board? Is it disabled through some other means?
Thanks.
Hi Tushar,
That's correct, same topic.
Yes, it can be closed here.
Thanks.
Hi Stevon
I think you have raised new ticket in nxp as "PCIe inaccessible in s32v234 boards" . this both ticket are same. can we close here and continue in nxp support ?
Regards ,
Tushar