Can I use TJA1040 to communicate with a Single Wire CAN device ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use TJA1040 to communicate with a Single Wire CAN device ?

1,012 Views
danielflor
Contributor III

Can I use one of the lines of CAN HS (CANH for example) to communicate on a Single Wire CAN bus in a compatible way ? By "compatible" I mean that the whole system should support valid SAEJ2411 baud rates, If so, what is the recommended way of doing it ? Specifically, should CANL be left floating, connected to ground, or something else?

Tags (1)
1 Reply

939 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, you cannot. Single Wire CAN is different physical layer.

You need to use single wire transceiver; MC33897 | Single-Wire Can Transceiver | NXP 

BR, Petr