BT656 640x480@60Hz GRAY parallel 8bit data process in i.mx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BT656 640x480@60Hz GRAY parallel 8bit data process in i.mx6q

394 Views
hwkwon1
Contributor II

Dear NXP Community

My board design was done using the i.mx6q board.
The BSP I use is:
yocto version : 5.4.70
kernel version: 4.9.11 or 5.15.32

The configuration diagram of the current product is as follows:
There is a thermal camera and FPGA in front of the i.mx6q, and FPGA output is BT656 640x480@60Hz GRAY 8bit parallel data.
This data is connected to i.mx6q EIM IPU2_CSI1 port.


1. Is it possible for i.mx6q to receive BT656 640x480@60Hz GRAY 8bit data input and perform BT656 decoding?
2. The input is 640x480@60Hz. Is it possible to process 60fps?

Best Regards,
Kwon

0 Kudos
Reply
2 Replies

358 Views
hwkwon1
Contributor II

Dear NXP TechSupport

Thank you for your answer.

0 Kudos
Reply

379 Views
joanxie
NXP TechSupport
NXP TechSupport

1. Is it possible for i.mx6q to receive BT656 640x480@60Hz GRAY 8bit data input and perform BT656 decoding?

>yes, can support BT656 interlaced mode or progressive mode, more detailed settings, pls refer to the enclosed AN


2. The input is 640x480@60Hz. Is it possible to process 60fps?

>yes, refer to the reference manual, Two parallel camera ports (up to 20-bit, up to 240MHz peak each).

0 Kudos
Reply