An urgent question about LSYNC loop length on MPC8548

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An urgent question about LSYNC loop length on MPC8548

364 Views
jooyi
Contributor I

Our board based on the MPC8548E has no problem at room temperature, but boot failure occurs at low temperature.
In relation to this, we are debugging the local bus part where the boot flash memory is connected.
According to the MPC8548 data sheet, the length of the LSYNC_IN/OUT signals should be the same as the longest of the LCLKs.
However, our board does not use LCLK signals and is in NC (floating) state.
I would appreciate it if you could tell me how to determine the length of the LSYNC_in/out loop signal in this case.

0 Kudos
Reply
1 Reply

354 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @jooyi,

 

LSYNC_IN needs to be directly connected to LSYNC_OUT. There is no such recomendation for length if not used.

In your case, please check the status of TRST pin. It should be tied to HRESET through a 0-kΩ resistor.

 

Regards,

Mrudang Shelat

0 Kudos
Reply