我們公司產品主要以MKL26Z128VLH4設計,近期因為SRAM不夠開發新功能,所以更換為MKL26Z256VLH4。但是在燒入過程無法燒入,想請教MKL26Z256VLH4的檔案哪邊可以找到?
謝謝。
您好,我已經改過IAR上型號的部分以下是Error Message,請問是哪裡出問題(已經改過MCU型號)?
可以参考Got an error in iAR with MKE14F ,"Error[LP011]: section placement failed"里的答复检查你的linker script。
Hi
这是参考手册Kinetis KL26: 48MHz Arm® Cortex®-M0+ 32-256KB Flash 32-121pin
请问你们使用的是哪个IDE?如果是NXP的MCUXpresso IDE+SDK,那么可以在MCU Settings里修改型号和存储配置:
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Robin_Shen:
您好,我們使用的IDE是IAR,首設上也詳細說明family之間彼此是相容的,我這邊面臨的問題是軟體無法燒錄的MCU(IDE環境MCU型号和存储配置不知道如何更改?)。
麻煩請教一下,謝謝。
请问是否已经将Device修改成MKL26Z256VLH4?
我对IAR不怎么熟悉,如果还是不行的话,建议新建一个MKL26Z256VLH4的工程将旧的工程移植进去。