JS16 OSBDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JS16 OSBDM

1,910 Views
Michael_Theisse
Contributor I

Hallo,

 

refering to USBDM_SOIC_JS16(Minimal):

 

Is it right that BKGD_DRV is connected to input- and output pins on MC9S08JS16CWJ. BKGD_DRV drives only an input pin on U1B (74LV125AD)?

Tags (2)
0 Kudos
Reply
1 Reply

1,088 Views
pgo
Senior Contributor V

Dear Michael,

 

The connections are correct.

 

The two pins are used as outputs to control the buffer at different times with the other pin 3-state.  Neither is actually used as an input.

 

This allows for faster manipulation of multiple port pins on a shared port but also allows independent control using a separate pin.

 

bye

 

0 Kudos
Reply