Dear All,
I have attached an updated version of the OSBDM code targeted to a JM60 which I hope will be of interest. However it has been extensively modified and is really intended for extended hardware. It should be usuable with more basic OSBDM hardware with some (hopefully simple) modification. It also requires a modified opensourcebdm.dll file to support the extra featrures..
It doesn't provide any advantages over the JB16 version apart from an increased range of BDM interface speeds.
bye
Dear All,
Attached is an updated version of USBDM for JM60 (see earlier post).
It now includes support for Flexis (Coldfire V1) parts. Experimental!
I note that there has been an "official" update of the OSBDM so this may now be moot.
bye
Hi, I'm a die-hard :smileyhappy: I am very pleased with the circuit and software which I built with parts laying around. I used a 74HC125 dip and a 2N3904 and 2N3906 for the power on/off circuit (3.3volts only). I am able to link up with an MC9S08QD4 quite readily and I love it.
Here's my question. When I turn on the Periodical Update for a Ram variable it returns 0xFF's while running. As soon as I halt the process, the correct value appears for the variable. I wonder if the hardware is at fault or perhaps that particular function may have a bug. I've attached a dump of the commands, and as you can see the periodic update returns FF's but the correct value is retrieved after the Halt. Thanks very much for your assistance, and I really appreciate your JM60 project.
Regards,
John H. Fisher
Dear All,
Attached is an updated version of USBDM for JMxx (see earlier posts).
It now allows firmware updates using in-circuit-programming over USB. This doesn't avoid the problem of needing a BDM to do the initial programming but does allow later updates without a bdm.
A version for the JM16CLC is also provided as well as one suitable for JM16/32/60CLD.
bye
Message Edited by pgo on 2008-08-14 09:43 AM
Message Edited by pgo on 2008-08-14 09:44 AM
Message Edited by pgo on 2008-08-14 09:46 AM
Message Edited by pgo on 2008-08-14 09:49 AM