i.MX 8M Nano integrates PN7160 startup failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Nano integrates PN7160 startup failed

2,040 Views
dx1
Contributor II

I'm trying to port PN7160 to i.MX 8M Nano Evaluation Kit | NXP Semiconductors

When I porting complete follow《AN13189-PN7160 Android porting guide》.The device will automatically restart after booting.

I have tried 2 different Android versions(android-13.0.0_1.0.0 & android-12.1.0_1.0.0), the problem is the same.

The following description can be seen from the startup log.

[2023/7/4 10:03:50] [   32.922292][    T1] init: starting service 'vendor.nfc_hal_service'...
[2023/7/4 10:03:50] [   32.955690][    T1] init: starting service 'bootanim'...
[2023/7/4 10:03:50] [   32.983711][    T1] init: Control message: Processed ctl.start for 'bootanim' from pid: 455 (/system/bin/surfaceflinger)
[2023/7/4 10:03:50] [   33.114696][  T283] logd: logdr: UID=1027 GID=1027 PID=612 n tail=0 logMask=8 pid=606 start=0ns deadline=0ns
[2023/7/4 10:03:50] [   33.126380][  T283] logd: logdr: UID=1027 GID=1027 PID=612 n tail=0 logMask=1 pid=606 start=0ns deadline=0ns
[2023/7/4 10:03:50] [   33.169961][    T1] init: Untracked pid 612 exited with status 0
[2023/7/4 10:03:50] [   33.176235][    T1] init: Untracked pid 612 did not have an associated service entry and will not be reaped
[2023/7/4 10:03:50] [   33.186900][    T1] init: Service 'vendor.nfc_hal_service' (pid 606) received signal 6
[2023/7/4 10:03:50] [   33.195279][    T1] init: Sending signal 9 to service 'vendor.nfc_hal_service' (pid 606) process group...
[2023/7/4 10:03:50] [   33.205886][    T1] libprocessgroup: Successfully killed process cgroup uid 1027 pid 606 in 0ms
[2023/7/4 10:03:50] [   33.218814][    T1] init: Untracked pid 614 exited with status 0
[2023/7/4 10:03:50] [   33.225348][    T1] init: Untracked pid 614 did not have an associated service entry and will not be reaped

 

0 Kudos
Reply
10 Replies

990 Views
mbz
Contributor I

Hello all,

I've encountered the same issue with the pn7220, could you please share the patch?

 

regards

0 Kudos
Reply

1,961 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @dx1 

Could you please share the steps to reproduce the issue?

 

Regards

Daniel

0 Kudos
Reply

1,953 Views
dx1
Contributor II

Hi @danielchen 

FYI. Thanks!

1,869 Views
danielchen
NXP TechSupport
NXP TechSupport

@dx1 

 

I will send you a patch to your email address.  later today.  You can integrate it and try it again.

 

Regards

Daniel

0 Kudos
Reply

1,815 Views
dx1
Contributor II

Hi @danielchen 

Have you already sent the patch? I haven't received it yet.

0 Kudos
Reply

1,764 Views
danielchen
NXP TechSupport
NXP TechSupport

 I sent it , please check your email

0 Kudos
Reply

1,733 Views
dx1
Contributor II

The patch are well received, thank you.

0 Kudos
Reply

1,839 Views
dx1
Contributor II

OK, Thank you so much! Is this patch for android13, or android12?

0 Kudos
Reply

1,765 Views
danielchen
NXP TechSupport
NXP TechSupport

tested with Android 13

0 Kudos
Reply

1,954 Views
dx1
Contributor II
 
0 Kudos
Reply