Problem Reading Mifare cards on PN532 Customized board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem Reading Mifare cards on PN532 Customized board.

1,582 Views
anmol_workmails
Contributor I

Antenna‌ pn532‌ NXP 

I have customized my own PN532 board.

1. For first assembly the board was working some time and some time it did not.(was getting i2c address , card read some time and other time it did not read the i2c address).without ground tap in antenna 

2. Second time same board i assembled i am able to read i2c every time. but it is not able to read any card.

      i tried nfc energy harvesting ic so without ground tap on antenna it showed no power, led glowed very less. then i ground tapped antenna so i was able to get full glow on LED on board energy harvesting ic. but still not able to read cards.

attaching the Schematic and board image

Tags (3)
0 Kudos
4 Replies

1,451 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please help us to provide more information on below questions:

1. May I ask what is the purpose of the yellow wire in front of the antenna?

pastedImage_5.png

2. Is this connected to a ground plane in the antenna on an inner layer?

3. Why are the inductors different, or is this a typo?

pastedImage_1.png

Best regards,

Ivan.

0 Kudos

1,451 Views
anmol_workmails
Contributor I

Hii Ivan 

1. The yellow wire is used to connect antenna ground tap to board ground that is VSS.
2. Its a double side PTH board no inner layer.
3. Its a typo value 560nh both.( i have corrected in schematic after attaching the files)
Also i wanted to ask they are TVSS1 AND TVSS2 transmitter ground on chip different from other ground(VSS). should i use them for antenna ground tapping while not shorting it to VSS (keeping them separate)
0 Kudos

1,451 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please remove the ground from the antenna, only the matching circuit is ok to ground it. Please measure the antenna parameters with a Network analyzer e.g. a MiniVNA and match it correctly to the front-end so that it is correctly tuned at 13,56 MHz. Also please refer to the antenna design guide available in the following link: https://www.nxp.com/docs/en/application-note/AN1445_An1444.zip 

Best regards,

Ivan.

0 Kudos

1,451 Views
anmol_workmails
Contributor I

Hii Ivan

1. The yellow wire is used to connect antenna ground tap to board ground

that is VSS.

2. Its a double side PTH board no inner layer.

3. Its a typo value 560nh both.( i have corrected in schematic after

attaching the files)

Also i wanted to ask they are TVSS1 AND TVSS2 transmitter ground on chip

different from other ground(VSS). should i use them for antenna ground

tapping while not shorting it to VSS (keeping them separate)

Thanks

Anmol Kohli

BTech-2016 Electronics Engineer

Embedded Design Engineer

m:+91-9958811944 e: anmol.workmails@gmail.com

0 Kudos