I have a CLEV6630A v2.0 that I am just trying to connect to NFC Cockpit v4.7.0 using USB and a Windows 8 machine. I have executed the install_vcom.bat successfully and see the device in Device Manager.
When starting NFC Cockpit I see errors right away. Please see screenshot.
I can then execute a "load protocol" and then an "rf Field On" command successfully. However, when I try to Activate Layer 3 or Activate Layer 4. I will continue to get HAL, IO_TIMEOUT errors.
Any thoughts?
I have a similar issue. I'm using some NTAG215 and have it directly on top of the device and get the same errors.
I'm using the default antenna and coil out of the box. Do you need to solder them since it seems like they are already connected.
EDIT: I managed to get it fixed by simply closing the port and reopening it a few times and closing NFC Cockpit and reopening it a few times. Weird.
Hello,
Please make sure that the corresponding tag is on the Reader's field so that it can activate layer 3 / 4.
Please let me know if you succeed.
Regards,
Ivan.