Porting PN7150 cannot read ID card(二代身份证) on Android platform.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting PN7150 cannot read ID card(二代身份证) on Android platform.

3,141件の閲覧回数
join_ren
Contributor III

Porting PN7150 cannot read ID card(二代身份证) on Android platform.

We test reading a TypeA card is OK.

Please tell us how to read the ID card. Thanks for your support.

0 件の賞賛
返信
7 返答(返信)

1,572件の閲覧回数
ethan_dang1
Contributor III

Hi @join_ren 

I'm having the same issue, have you already solved it

0 件の賞賛
返信

3,095件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @join_ren @yrn ,

 

I am not sure if you have got the latest patch for android 9.0, but anyway, you may create a private case for it. Please kindly tell me the case number when it is available.

 

https://community.nxp.com/t5/Using-Our-Community-Knowledge/How-to-submit-a-new-question-for-NXP-Supp... 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信

2,995件の閲覧回数
yrn
Contributor I

Dear Sir,

      I have create a new case :Case Number : 00335216.

       I have patch from AN11690( NXP NCI Android Porting Guidelines Rev. 2.0 — 14 December 2020 ). But it can not read ChinaID(TypeB).

        Please help me check it.

thanks and waitting for your answer.

0 件の賞賛
返信

2,986件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yrn ,

 

Thanks for the information! I have taken this case.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,114件の閲覧回数
yrn
Contributor I

Hi Sir,

    Thanks for your answer. I know how to get ChinaID information. First, reading a string from ChinaID. Second, Getting the full information of ChinaID by the string from server licensed by Ministry of Public Security. 

    But NOW, I can not read a string from ChinaID. the particial error log like below(Please check all of log in attached file.):

01-25 09:17:40.194 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(228)] NfcTag::IsSameKovio: enter
01-25 09:17:40.194 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(279)] NfcTag::discoverTechnologies (activation): enter
01-25 09:17:40.194 11192 11232 E libnfc_nci: [ERROR:NfcTag.cpp(385)] NfcTag::discoverTechnologies (activation): unknown protocol ????
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(391)] NfcTag::discoverTechnologies (activation): index=0; tech=-1; handle=1; nfc type=0
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(395)] NfcTag::discoverTechnologies (activation): exit
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(537)] NfcTag::createNativeNfcTag: enter
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(607)] NfcTag::fillNativeNfcTagMembers1
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(659)] NfcTag::fillNativeNfcTagMembers2
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(690)] NfcTag::fillNativeNfcTagMembers3: index=0; rf tech params mode=1
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(804)] NfcTag::fillNativeNfcTagMembers4: index=0
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(904)] NfcTag::fillNativeNfcTagMembers4: tech unknown ????
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(961)] NfcTag::fillNativeNfcTagMembers5: tech B
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(579)] NfcTag::createNativeNfcTag: try notify nfc service

==========================================================================================

 The patch of Android8.0 is OK. I compare the patch of Android9.0 referend by AN11690 with the patch of Android8.0. I found that the patch of Android9.0 does not involve the code processed ChinaID in Android8.0's patch. the processing ChinaID code involved the  compile switch of "#if(NXP_EXTNS == TRUE)". The patch of Android9.0 does not include these code.

So, Please help me check why the patch of Android9 can not work well and whether the issue core is "#if(NXP_EXTNS == TRUE)".

Thanks

Yang

  

0 件の賞賛
返信

3,127件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @join_ren ,

 

Would do you mean reading ID card? As far as I know, reading the content inside the ID card needs a special App licensed by the Ministry of Public Security.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,112件の閲覧回数
yrn
Contributor I

Hi Sir,

    Thanks for your answer. I know how to get ChinaID information. First, reading a string from ChinaID. Second, Getting the full information of ChinaID by the string from server licensed by Ministry of Public Security. 

    But NOW, I can not read a string from ChinaID. the particial error log like below(Please check all of log in attached file.):

01-25 09:17:40.194 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(228)] NfcTag::IsSameKovio: enter
01-25 09:17:40.194 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(279)] NfcTag::discoverTechnologies (activation): enter
01-25 09:17:40.194 11192 11232 E libnfc_nci: [ERROR:NfcTag.cpp(385)] NfcTag::discoverTechnologies (activation): unknown protocol ????
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(391)] NfcTag::discoverTechnologies (activation): index=0; tech=-1; handle=1; nfc type=0
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(395)] NfcTag::discoverTechnologies (activation): exit
01-25 09:17:40.195 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(537)] NfcTag::createNativeNfcTag: enter
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(607)] NfcTag::fillNativeNfcTagMembers1
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(659)] NfcTag::fillNativeNfcTagMembers2
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(690)] NfcTag::fillNativeNfcTagMembers3: index=0; rf tech params mode=1
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(804)] NfcTag::fillNativeNfcTagMembers4: index=0
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(904)] NfcTag::fillNativeNfcTagMembers4: tech unknown ????
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(961)] NfcTag::fillNativeNfcTagMembers5: tech B
01-25 09:17:40.196 11192 11232 I libnfc_nci: [INFO:NfcTag.cpp(579)] NfcTag::createNativeNfcTag: try notify nfc service

==========================================================================================

 The patch of Android8.0 is OK. I compare the patch of Android9.0 referend by AN11690 with the patch of Android8.0. I found that the patch of Android9.0 does not involve the code processed ChinaID in Android8.0's patch. the processing ChinaID code involved the  compile switch of "#if(NXP_EXTNS == TRUE)". The patch of Android9.0 does not include these code.

So, Please help me check why the patch of Android9 can not work well and whether the issue core is "#if(NXP_EXTNS == TRUE)".

Thanks

Yang Le

  

0 件の賞賛
返信