PN5180 SPI from esp32 core (Arduino ide) takes too long

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 SPI from esp32 core (Arduino ide) takes too long

1,513件の閲覧回数
oferrer
Contributor III

Hi, I implemented an iso15693 inventory16 command on an esp32 controller using Arduino IDE.

It works well, although collisions happen. But i had to delay flow control 1ms after asserting NSS before wait for busy pin high. If i didnt that it doesn't work.

The problem Is the inventory take almost a second for few tags. This Is a long time for my application. 

I tried microsecondsDelay with values under 1000us, but it didn't work either, inventory fails.

Pn5180 datasheet say nothing about this. Has anyone had this problem? 

Any help. Thanks in Advance.

 

0 件の賞賛
返信
0 返答(返信)