PN7462: How to use HSU port to communicate for the CCID example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462: How to use HSU port to communicate for the CCID example

647 次查看
shiv_patil
Contributor II

Hello Community,

I am working on the PN7462 NFC development board using the CCID example.

I would like to use the HSU port for communication instead of the USB port.

Will you please help me to know,

1. Is it possible to communicate over the HSU port using the CCID example?
2. Further we want to implement a serial bootloader over the HSU port, will HSU support the serial bootloader?

 

Regards,
Shiv Patil.

0 项奖励
回复
1 回复

622 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did you mean the PN7462 EVK. board? If yes. One can't use HSU port instead of USB Port.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

标记 (1)
0 项奖励
回复