PN7150 c11006

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7150 c11006

638 次查看
zhichaotan
Contributor I

hi,if the pn7150 hardware VS switch to c11006 from c11002, it is there anything need to modify in the Android system driver? can it be replaced directly?
thanks.

0 项奖励
回复
1 回复

634 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Both version of the difference is just a firmware update and this are backwards compatible,  Version C11006 ,PN7150B0HN/C11006 contains a firmware update compared to the previous version.
The firmware version is 10.01.AE and contains the following new features and fixes:
• Anti tearing mechanism: An Anti tearing mechanism has been added. For details,
please refer to the User Manual UM10936.
• A fix has been added that addresses a collision resolution problem for ISO 15693 tags
in case there are multiple tags in the field.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励
回复