hi,if the pn7150 hardware VS switch to c11006 from c11002, it is there anything need to modify in the Android system driver? can it be replaced directly?
thanks.
Hello,
Both version of the difference is just a firmware update and this are backwards compatible, Version C11006 ,PN7150B0HN/C11006 contains a firmware update compared to the previous version.
The firmware version is 10.01.AE and contains the following new features and fixes:
• Anti tearing mechanism: An Anti tearing mechanism has been added. For details,
please refer to the User Manual UM10936.
• A fix has been added that addresses a collision resolution problem for ISO 15693 tags
in case there are multiple tags in the field.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------