PN5321 saturate card at close proximity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5321 saturate card at close proximity

1,068件の閲覧回数
bernardvisser
Contributor I

We made a custom NFC reader / writer with the PN5321, copying the refrence design from AN10449_1.

We use Mifare Classic 4K cards in our application.

One of our prototypes is giving intermittent problems with card communication. We found that communicatoin with the card stops working if the card is too close to the antenna.

If the card is 6-15mm above the antenna (coil) communication is bad.

If the card is ~30mm away from the antenna communicaiton is reliable.

Any suggestions on what components to alter to reduce the field strength? 

ラベル(2)
タグ(1)
0 件の賞賛
返信
0 返答(返信)