Reader module for reading NDEF messages from Type B tags?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reader module for reading NDEF messages from Type B tags?

1,057 Views
manojrohitvempa
Contributor II

Hello guys,

I am trying to read NDEF message from ISO 14443 Type B tag using explore-NFC reader module. But the example programs are only demonstrated for type A tags. Could anyone suggest me any other NFC reader module compatible to raspberry pi which can read NDEF messages from type B tags.

Thank you in advance. 

0 Kudos
1 Reply

840 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to AN1425 in which they provide guidance on antenna and RF amplifier design, as you mentioned in the case, it is for devices such as PN5xx and MFRC52x for which the design is the same.

AN1425:

http://www.nxp.com/docs/en/application-note/AN1425_AN166510.zip

Best regards,

Ivan.

0 Kudos