NFC Cockpit not seeing OM25180FDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC Cockpit not seeing OM25180FDK

1,950 次查看
KevinBraun
Contributor I

Hello,

I have a brand new NFC Cockpit setup on a Windows 10 machine.  After a few struggles, I now have the USB COM port set up properly, NxpNfcCockpit VCOM (COM5). 

I installed NFC Cockpit on my D: drive,  D:\nxp\NxpNfcCockpit_v4.8.0.0\bin\NxpNfcCockpitGUI.exe

NFC Cockpit does not see the OM25180 board. Open Port, Soft Reset, etc. are greyed out and the Log Monitor shows nothing.

The board has a blue(PN_RST), green(IRQ), dull red(LD100) LED on and a flashing orange(LD200) LED

Thanks,

...kevin

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,766 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

It would be helpful to refer to chapter 3 of AN11744 regarding the necessary firmware for PN5180.

Hope this helps.

Have a nice day,

Ivan.

0 项奖励
回复